Plugin Commands: Comms Hub Function
Detailed Description
The comms-hub-function plugin contributes several CLI commands to the application framework to be used in configuring and managing the CHF.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CLOSE_TUNNEL |
plugin comms-hub-function close-tunnel [dstEUI64:8]
-
Remove the tunnel for a given device.
- dstEUI64 - IEEE_ADDRESS
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_CREATE_TUNNEL |
plugin comms-hub-function create-tunnel [dstEUI64:8] [endpoint:1]
-
Create tunnel for the given device and endpoint.
- dstEUI64 - IEEE_ADDRESS
- endpoint - INT8U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_GET_TUNNEL_ENDPOINT |
plugin comms-hub-function get-tunnel-endpoint [nodeId:2]
-
Retrieve the tunneling endpoint for a given nodeId.
- nodeId - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT |
plugin comms-hub-function print
- Prints the comms hub tunnel table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_PRINT_SUPPORTED_USE_CASES |
plugin comms-hub-function print-supported-use-cases
- Print the list of supported use cases. The message code printed should be used with the simulate-gbz-msg command.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SEND |
plugin comms-hub-function send [dstEUI64:8] [payload:-1]
-
Send a message.
- dstEUI64 - IEEE_ADDRESS
- payload - OCTET_STRING
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_SIMULATE_GBZ_MSG |
plugin comms-hub-function simulate-gbz-msg [dstEUI64:8] [useCase:2]
-
Simulate transmission of a GBZ message to the Comms Hub Function.
- dstEUI64 - IEEE_ADDRESS
- useCase - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_PLUGIN_COMMS_HUB_FUNCTION_TIMEOUT |
plugin comms-hub-function timeout [timeout:4]
-
Set the default sleepy message timeout.
- timeout - INT32U