Plugin Commands: Green Power Client
Detailed Description
The Green Power Client plugin contributes CLI commands to the application framework to be used for getting, setting, and displaying information relevant to the Green Power Client cluster.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_GROUP_SINK |
plugin green-power-client add-group-sink [sourceID:4] [sinkGroup:2]
-
Add a groupcast sink for a given GPD
- sourceID - INT32U - GPD Source ID
- sinkGroup - INT16U - Sink group
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_SINK |
plugin green-power-client add-sink [sourceID:4] [sinkIeee:8]
-
Add a sink for a given GPD
- sourceID - INT32U - GPD Source ID
- sinkIeee - IEEE_ADDRESS - Sink's IEEE address
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_CLEAR_PROXY_TABLE |
plugin green-power-client clear-proxy-table
- clear the proxy table
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_DUPLICATE_FILTER_TEST |
plugin green-power-client duplicate-filter-test [endpoint:1] [sourceId:4] [sequenceNumber:1]
-
This is used to instrument the current device receiving a message in order to test the duplicate message filtering functionality.
- endpoint - INT8U
- sourceId - INT32U - source Id of the fake incoming message
- sequenceNumber - INT8U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_PRINT_PROXY_TABLE |
plugin green-power-client print-proxy-table
- Print the proxy table
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_GPD |
plugin green-power-client rm-gpd [sourceID:4]
-
Remove a given GPD from the proxy table
- sourceID - INT32U - GPD Source ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_SINK |
plugin green-power-client rm-sink [sourceID:4] [sinkIeee:8]
-
remove a sink for a given GPD. If that's the last sink, remove the proxy table entry
- sourceID - INT32U - GPD Source ID
- sinkIeee - IEEE_ADDRESS - Sink's IEEE address
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_KEY |
plugin green-power-client set-key [index:1] [key:16]
-
This is used to set the key for a proxy table entry
- index - INT8U
- key - SECURITY_KEY - source Id of the fake incoming message
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_PROXY_ENTRY |
plugin green-power-client set-proxy-entry [index:1] [sourceID:4] [sinkNodeId:2] [options:4]
-
Set a proxy table entry
- index - INT8U - index to proxy table
- sourceID - INT32U - GPD Source ID
- sinkNodeId - INT16U - Sink's node address
- options - INT32U