Plugin Commands: Device Database
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_ADD_DUMMY |
|
plugin device-database device add-dummy [eui64:8] [endpoints:1] [clusters:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_ERASE |
|
plugin device-database device erase [eui64:8]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_PRINT |
|
plugin device-database device print [eui64:8]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_PRINT_ALL |
|
plugin device-database print-all
|
|
Detailed Description
This plugin provides a set of CLI commands for printing and manipulating the device database.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_ADD_DUMMY |
plugin device-database device add-dummy [eui64:8] [endpoints:1] [clusters:2]
-
Add a device with specified EUI64 and a sequential number of clusters and endpoints.
- eui64 - IEEE_ADDRESS - The address of the dummy device to add.
- endpoints - INT8U - The number of dummy endpoints to add.
- clusters - INT16U - The number of dummy clusters to add.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_ERASE |
plugin device-database device erase [eui64:8]
-
Erase the device with specified EUI64 from the database.
- eui64 - IEEE_ADDRESS - The address of the device to erase from the database.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_DEVICE_PRINT |
plugin device-database device print [eui64:8]
-
Print all the clusters and endpoints known about the specified device in the database.
- eui64 - IEEE_ADDRESS - The address of the device to be looked up (little endian)
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_DATABASE_PLUGIN_DEVICE_DATABASE_PRINT_ALL |
plugin device-database print-all
- Print all devices in the database.