Cluster Commands: SL Works With All Hubs
Detailed Description
This group describes the CLI commands for the SL Works With All Hubs cluster. Listed below is a description of the cluster:
Silicon Labs proprietary attributes and commands for Works With All Hubs functional extensions.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_CLEAR_BINDING_TABLE |
zcl sl-wwah clear-binding-table
- Clear the binding table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_APP_EVENT_RETRY_ALG |
zcl sl-wwah disable-app-event-retry-alg
- Disable WWAH App Event retry algorithm.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_APS_LINK_KEY_AUTH |
zcl sl-wwah disable-aps-link-key-auth [numberExemptClusters:1] [clusterId:2]
-
Disable enforcement of APS-level security for all cluster commands.
- numberExemptClusters - INT8U
- clusterId - CLUSTER_ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_BAD_PARENT_RECOVERY |
zcl sl-wwah disable-bad-parent-recovery
- Disable WWAH Bad Parent Recovery feature.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_CONFIG_MODE |
zcl sl-wwah disable-config-mode
- Disable Configuration Mode.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_MGMT_LEAVE_WO_REJOIN |
zcl sl-wwah disable-mgmt-leave-wo-rejoin
- Causes device to ignore MGMT Leave Without Rejoin commands.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_OTA_DOWNGRADES |
zcl sl-wwah disable-ota-downgrades
- Disallow OTA downgrade of all device firmware components.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_PARENT_CLASSIFY |
zcl sl-wwah disable-parent-classify
- Disable WWAH Parent Classification advertisements.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_REJOIN_ALG |
zcl sl-wwah disable-rejoin-alg
- Disable WWAH rejoin algorithm.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_REQUIRE_APS_ACK_UNICAST |
zcl sl-wwah disable-require-aps-ack-unicast
- Roll back changes made by Require APS ACK on Unicasts.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_ROUTER_CHECKINS |
zcl sl-wwah disable-router-checkins
- Disable device from periodically checking connectivity with Zigbee Coordinator.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_DISABLE_TL_INTERPAN_MSG_SUPPORT |
zcl sl-wwah disable-tl-interpan-msg-support
- Causes device to ignore Touchlink Interpan messages.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_APP_EVENT_RETRY_ALG |
zcl sl-wwah enable-app-event-retry-alg [firstBackoffTimeSeconds:1] [backoffSeqCommonRatio:1] [maxBackoffTimeSeconds:4] [maxRedeliveryAttempts:1]
-
Enable WWAH App Event retry algorithm.
- firstBackoffTimeSeconds - INT8U
- backoffSeqCommonRatio - INT8U
- maxBackoffTimeSeconds - INT32U
- maxRedeliveryAttempts - INT8U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_APS_LINK_KEY_AUTH |
zcl sl-wwah enable-aps-link-key-auth [numberExemptClusters:1] [clusterId:2]
-
Enable enforcement of APS-level security for all cluster commands.
- numberExemptClusters - INT8U
- clusterId - CLUSTER_ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_BAD_PARENT_RECOVERY |
zcl sl-wwah enable-bad-parent-recovery
- Enable WWAH Bad Parent Recovery feature.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_CONFIG_MODE |
zcl sl-wwah enable-config-mode
- Enable Configuration Mode.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_PARENT_CLASSIFY |
zcl sl-wwah enable-parent-classify
- Enable WWAH Parent Classification advertisements.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_REJOIN_ALG |
zcl sl-wwah enable-rejoin-alg [fastRejoinTimeoutSeconds:2] [durationBetweenRejoinsSeconds:2] [fastRejoinFirstBackoffSeconds:2] [maxBackoffTimeSeconds:2] [maxBackoffIterations:2]
-
Enable WWAH rejoin algorithm.
- fastRejoinTimeoutSeconds - INT16U
- durationBetweenRejoinsSeconds - INT16U
- fastRejoinFirstBackoffSeconds - INT16U
- maxBackoffTimeSeconds - INT16U
- maxBackoffIterations - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_REQUIRE_APS_ACK_UNICAST |
zcl sl-wwah enable-require-aps-ack-unicast [numberExemptClusters:1] [clusterId:2]
-
Require all unicast commands to have APS ACKs enabled.
- numberExemptClusters - INT8U
- clusterId - CLUSTER_ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_ROUTER_CHECKINS |
zcl sl-wwah enable-router-checkins [checkInInterval:2]
-
Enable device to periodically check connectivity with Zigbee Coordinator.
- checkInInterval - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_ENABLE_TC_SEC_NTWK_KEY_ROT |
zcl sl-wwah enable-tc-sec-ntwk-key-rot
- Process only network key rotation commands sent via unicast and encrypted by Trust Center Link Key.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_QUERY_APS_ACK_REQUIREMENT |
zcl sl-wwah query-aps-ack-requirement
- Query whether unicast commands are required to have APS ACKs enabled.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_QUERY_APS_LINK_KEY_AUTH |
zcl sl-wwah query-aps-link-key-auth [clusterId:2]
-
Query status of APS-level security enforcement for a specified cluster.
- clusterId - CLUSTER_ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_QUERY_DEBUG_REPORT |
zcl sl-wwah query-debug-report [debugReportId:1]
-
Query for specified debug report.
- debugReportId - INT8U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_QUERY_TC_FOR_CLUSTER_SERVER |
zcl sl-wwah query-tc-for-cluster-server
- Causes device to send an appropriate Trust Center for Cluster Server Query Response command.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_REQ_TIME |
zcl sl-wwah req-time
- Trigger device to request current attribute values from Time Cluster server.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_REQUEST_NEW_APS_LINK_KEY |
zcl sl-wwah request-new-aps-link-key
- Trigger device to request a new APS link key from the Trust Center.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_SET_IAS_ENROLL_METHOD |
zcl sl-wwah set-ias-enroll-method [enrollmentMode:1]
-
Set the enrollment method of an IAS Zone server.
-
enrollmentMode - WwahIasZoneEnrollmentMode [ENUM8]
- See also
- EmberAfWwahIasZoneEnrollmentMode
-
enrollmentMode - WwahIasZoneEnrollmentMode [ENUM8]
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_SET_MAC_POLL_CCA_WAIT_TIME |
zcl sl-wwah set-mac-poll-cca-wait-time [waitTime:1]
-
Set MAC poll CCA wait time.
- waitTime - INT8U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_SET_PENDING_NETWORK_UPDATE |
zcl sl-wwah set-pending-network-update [channel:1] [panId:2]
-
Set pending network update parameters.
- channel - INT8U
- panId - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_SURVEY_BEACONS |
zcl sl-wwah survey-beacons [standardBeacons:1]
-
Causes device to perform a scan for beacons advertising the device's network.
- standardBeacons - BOOLEAN
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_S_L_WORKS_WITH_ALL_HUBS_USE_TC_FOR_CLUSTER_SERVER |
zcl sl-wwah use-tc-for-cluster-server [numberOfClusters:1] [clusterId:2]
-
Use only the Trust Center as cluster server for the set of clusters specified.
- numberOfClusters - INT8U
- clusterId - CLUSTER_ID