Detailed Description
The Informational command set provides commands for displaying information about the device. These commands include things like printing out the attribute tablerr
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_DEBUGPRINT_ALL_OFF |
debugprint all_off
- Turns off all debug printing
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_DEBUGPRINT_ALL_ON |
debugprint all_on
- Turns on all compiled in debug printing
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_DEBUGPRINT_OFF |
debugprint off [area:1]
-
Turns off compiled in debug printing for a specific debug printing area. Debug print areas are defined in the generated <application>.h header file.
- area - INT8U - The debug area mask listed in the <application>.h file
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_DEBUGPRINT_ON |
debugprint on [area:1]
-
Turns on compiled in debug printing for a specific debug printing area. Debug print areas are defined in the generated <application>.h header file.
- area - INT8U - The debug area mask listed in the <application>.h file
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_DEBUGPRINT_STATUS |
debugprint status
- Prints out the current settings for debug printing on the device
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_HELP |
help
- Prints out the cli command options for the device
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_INFO |
info
- Gives information about the local node
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_LIBS |
libs
- Lists which optional libraries of the stack are implemented on this device
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_OPTION_BINDING_TABLE_PRINT |
option binding-table print
- Prints out the binding table to the command line.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_OPTION_PRINT_RX_MSGS_DISABLE |
option print-rx-msgs disable
- Disable the printing of received messages.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_OPTION_PRINT_RX_MSGS_ENABLE |
option print-rx-msgs enable
- Enable the printing of received messages.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_PRINT_ATTR |
print attr
- Print the attribute table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_PRINT_ENTROPY_SOURCE |
print entropy source
- Print the the entropy source that is used for true random number generation.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_PRINT_TIME |
print time
- Print out the time information
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_INFO_VERSION |
version
- Shows the version of the software