EmberBeaconData Struct Reference
Defines a beacon entry that is processed when scanning, joining, or rejoining.
#include <
ember-types.h
>
Data Fields | |
uint8_t | channel |
uint8_t | lqi |
int8_t | rssi |
uint8_t | depth |
uint8_t | nwkUpdateId |
int8_t | power |
int8_t | parentPriority |
bool | enhanced: 1 |
bool | permitJoin: 1 |
bool | hasCapacity: 1 |
EmberPanId | panId |
EmberNodeId | sender |
uint8_t | extendedPanId [EXTENDED_PAN_ID_SIZE] |
Defines a beacon entry that is processed when scanning, joining, or rejoining.
Field Documentation
uint8_t EmberBeaconData::channel |
uint8_t EmberBeaconData::depth |
bool EmberBeaconData::enhanced |
uint8_t EmberBeaconData::extendedPanId[EXTENDED_PAN_ID_SIZE] |
bool EmberBeaconData::hasCapacity |
uint8_t EmberBeaconData::lqi |
uint8_t EmberBeaconData::nwkUpdateId |
EmberPanId EmberBeaconData::panId |
int8_t EmberBeaconData::parentPriority |
bool EmberBeaconData::permitJoin |
int8_t EmberBeaconData::power |
int8_t EmberBeaconData::rssi |
EmberNodeId EmberBeaconData::sender |
The documentation for this struct was generated from the following file:
ember-types.h