EmberAfMessageStruct Struct Reference
The EmberAfMessageStruct is a struct wrapper that contains all the data about a low-level message to be sent (it may be ZCL or may be some other protocol).
#include <
af-types.h
>
Data Fields |
|
| EmberAfMessageSentFunction | callback |
| EmberApsFrame * | apsFrame |
| uint8_t * | message |
| uint16_t | indexOrDestination |
| uint16_t | messageLength |
| EmberOutgoingMessageType | type |
| bool | broadcast |
The EmberAfMessageStruct is a struct wrapper that contains all the data about a low-level message to be sent (it may be ZCL or may be some other protocol).
Field Documentation
| EmberApsFrame * EmberAfMessageStruct::apsFrame |
| bool EmberAfMessageStruct::broadcast |
| EmberAfMessageSentFunction EmberAfMessageStruct::callback |
| uint16_t EmberAfMessageStruct::indexOrDestination |
| uint8_t* EmberAfMessageStruct::message |
| uint16_t EmberAfMessageStruct::messageLength |
| EmberOutgoingMessageType EmberAfMessageStruct::type |
The documentation for this struct was generated from the following file:
-
af-types.h