EmberNeighborTableEntry Struct Reference
Defines an entry in the neighbor table.
#include <
ember-types.h
>
Data Fields | |
uint16_t | shortId |
uint8_t | averageLqi |
uint8_t | inCost |
uint8_t | outCost |
uint8_t | age |
EmberEUI64 | longId |
Defines an entry in the neighbor table.
A neighbor table entry stores information about the reliability of RF links to and from neighboring nodes.
Field Documentation
uint8_t EmberNeighborTableEntry::age |
In EmberZNet Pro, the number of aging periods elapsed since a neighbor exchange message was last received from this neighbor. In stack profile 1, the number of aging periods since any packet was received. An entry with an age greater than 3 is considered stale and may be reclaimed. The aging period is 16 seconds.
uint8_t EmberNeighborTableEntry::averageLqi |
An exponentially weighted moving average of the link quality values of incoming packets from this neighbor as reported by the PHY.
uint8_t EmberNeighborTableEntry::inCost |
The incoming cost for this neighbor, computed from the average LQI. Values range from 1 for a good link to 7 for a bad link.
EmberEUI64 EmberNeighborTableEntry::longId |
The 8 byte EUI64 of the neighbor.
uint8_t EmberNeighborTableEntry::outCost |
The outgoing cost for this neighbor, obtained from the most recently received neighbor exchange message from the neighbor. A value of zero means that a neighbor exchange message from the neighbor has not been received recently enough, or that our ID was not present in the most recently received one. EmberZNet Pro only.
uint16_t EmberNeighborTableEntry::shortId |
The neighbor's two-byte network ID.
The documentation for this struct was generated from the following file:
ember-types.h