Cluster Commands: Thermostat
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SET |
|
zcl tstat set [mode:1] [amount:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SWS |
|
zcl tstat sws [numberOfTransitionsForSequence:1] [dayOfWeekForSequence:1] [modeForSequence:1] [payload:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GWS |
|
zcl tstat gws [daysToReturn:1] [modeToReturn:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_CWS |
|
zcl tstat cws
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GRS |
|
zcl tstat grs
|
|
Detailed Description
This group describes the CLI commands for the Thermostat cluster. Listed below is a description of the cluster:
An interface for configuring and controlling the functionality of a thermostat.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_CWS |
zcl tstat cws
- The Clear Weekly Schedule command is used to clear the weekly schedule.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GRS |
zcl tstat grs
- The Get Relay Status Log command is used to query the thermostat internal relay status log.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GWS |
zcl tstat gws [daysToReturn:1] [modeToReturn:1]
-
Command description for GetWeeklySchedule
- daysToReturn - DayOfWeek [BITMAP8]
- modeToReturn - ModeForSequence [BITMAP8]
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SET |
zcl tstat set [mode:1] [amount:1]
-
Command description for SetpointRaiseLower
- mode - SetpointAdjustMode [ENUM8]
-
amount - INT8S
- See also
- EmberAfSetpointAdjustMode
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SWS |
zcl tstat sws [numberOfTransitionsForSequence:1] [dayOfWeekForSequence:1] [modeForSequence:1] [payload:1]
-
Command description for SetWeeklySchedule
- numberOfTransitionsForSequence - ENUM8
- dayOfWeekForSequence - DayOfWeek [BITMAP8]
- modeForSequence - ModeForSequence [BITMAP8]
- payload - INT8U