EmberAfDeviceManagementSiteId Struct Reference
#include <
af-types.h
>
Data Fields |
|
| uint8_t | siteId [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1] |
| uint32_t | implementationDateTime |
| uint32_t | issuerEventId |
Field Documentation
| uint32_t EmberAfDeviceManagementSiteId::implementationDateTime |
| uint32_t EmberAfDeviceManagementSiteId::issuerEventId |
| uint8_t EmberAfDeviceManagementSiteId::siteId[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1] |
The documentation for this struct was generated from the following file:
-
af-types.h