EmberAfGbzMessageData Struct Reference
#include <
af-types.h
>
Data Fields |
|
| bool | encryption |
| uint8_t * | plainPayload |
| uint16_t | plainPayloadLength |
| uint8_t * | encryptedPayload |
| uint16_t | encryptedPayloadLength |
Field Documentation
| uint8_t* EmberAfGbzMessageData::encryptedPayload |
| uint16_t EmberAfGbzMessageData::encryptedPayloadLength |
| bool EmberAfGbzMessageData::encryption |
| uint8_t* EmberAfGbzMessageData::plainPayload |
| uint16_t EmberAfGbzMessageData::plainPayloadLength |
The documentation for this struct was generated from the following file:
-
af-types.h