Plugin Commands: Key Establishment
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_INTERPAN |
|
plugin key-establishment interpan [panId:2] [eui64:-1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_START |
|
plugin key-establishment start [nodeId:2] [endpoint:1]
|
|
Detailed Description
The Key Establishment commands provide commands to initiate key establishment with a remote target.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_INTERPAN |
plugin key-establishment interpan [panId:2] [eui64:-1]
-
Initiate key establishment with the target device over interpan.
- panId - INT16U - The PAN ID that the target is located on.
- eui64 - OCTET_STRING - The target's EUI64 (big endian)
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_START |
plugin key-establishment start [nodeId:2] [endpoint:1]
-
Initiates key establishment with the target node ID.
- nodeId - INT16U - Target node ID.
- endpoint - INT8U - Target node's endpoint.