Plugin Commands: Simple Metering Server
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_SERVER_PLUGIN_SIMPLE_METERING_SERVER_CONFIGURE_MIRROR |
|
plugin simple-metering-server configure-mirror [client:2] [serverEndpoint:1] [clientEndpoint:1] [IssuerEventId:4] [ReportingInterval:4] [mirrorNotificationReporting:1] [NotificationScheme:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_SERVER_PLUGIN_SIMPLE_METERING_SERVER_TOGGLE_FAST_POLL_MODE |
|
plugin simple-metering-server toggle-fast-poll-mode [enableFastPolling:1]
|
|
Detailed Description
The simple-metering-server plugin contributes CLI commands to the application framework to be used in conjunction with the Simple Metering cluster in a server context
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_SERVER_PLUGIN_SIMPLE_METERING_SERVER_CONFIGURE_MIRROR |
plugin simple-metering-server configure-mirror [client:2] [serverEndpoint:1] [clientEndpoint:1] [IssuerEventId:4] [ReportingInterval:4] [mirrorNotificationReporting:1] [NotificationScheme:1]
-
Send configure mirror command to Metering client.
- client - INT16U - The network address of the server to which the request will be sent.
- serverEndpoint - INT8U - The local endpoint from which the request will be sent.
- clientEndpoint - INT8U - The remote endpoint to which the request will be sent.
- IssuerEventId - INT32U - The issuer event Id as specified by the device.
- ReportingInterval - INT32U - 3 bytes of Reporting Interval value.
- mirrorNotificationReporting - INT8U - Mirror Notification Reporting value
- NotificationScheme - INT8U - Mirror Notification Reporting value
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_SERVER_PLUGIN_SIMPLE_METERING_SERVER_TOGGLE_FAST_POLL_MODE |
plugin simple-metering-server toggle-fast-poll-mode [enableFastPolling:1]
-
Disable fast polling mode for testing.
- enableFastPolling - INT8U - 1 to enable, 0 to disable fast polling mode.