EmberAfDeviceManagementSupplier Struct Reference
#include <
af-types.h
>
Data Fields |
|
| uint32_t | proposedProviderId |
| uint32_t | implementationDateTime |
| uint32_t | providerChangeControl |
| uint8_t | proposedProviderName [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH +1] |
| uint8_t | proposedProviderContactDetails [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH +1] |
Field Documentation
| uint32_t EmberAfDeviceManagementSupplier::implementationDateTime |
| uint8_t EmberAfDeviceManagementSupplier::proposedProviderContactDetails[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH +1] |
| uint32_t EmberAfDeviceManagementSupplier::proposedProviderId |
| uint8_t EmberAfDeviceManagementSupplier::proposedProviderName[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH +1] |
| uint32_t EmberAfDeviceManagementSupplier::providerChangeControl |
The documentation for this struct was generated from the following file:
-
af-types.h