EmberAfPluginMessagingClientMessage Struct Reference
#include <
af-types.h
>
Data Fields |
|
| bool | valid |
| bool | active |
| EmberAfPluginEsiManagementBitmask | esiBitmask |
| uint8_t | clientEndpoint |
| uint32_t | messageId |
| uint8_t | messageControl |
| uint32_t | startTime |
| uint32_t | endTime |
| uint16_t | durationInMinutes |
| uint8_t | message [ EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE +1] |
Field Documentation
| bool EmberAfPluginMessagingClientMessage::active |
| uint8_t EmberAfPluginMessagingClientMessage::clientEndpoint |
| uint16_t EmberAfPluginMessagingClientMessage::durationInMinutes |
| uint32_t EmberAfPluginMessagingClientMessage::endTime |
| EmberAfPluginEsiManagementBitmask EmberAfPluginMessagingClientMessage::esiBitmask |
| uint8_t EmberAfPluginMessagingClientMessage::message[ EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE +1] |
| uint8_t EmberAfPluginMessagingClientMessage::messageControl |
| uint32_t EmberAfPluginMessagingClientMessage::messageId |
| uint32_t EmberAfPluginMessagingClientMessage::startTime |
| bool EmberAfPluginMessagingClientMessage::valid |
The documentation for this struct was generated from the following file:
-
af-types.h