Plugin Commands: Barrier Control Server Cluster
Detailed Description
Commands pertaining to the Silicon Labs Barrier Control server cluster.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_CLOSE |
plugin barrier-control-server close [endpoint:1]
-
Notify the plugin that the barrier has been closed manually.
- endpoint - INT8U - The endpoint on which the barrier has been closed
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_FAILED_COMMUNICATION |
plugin barrier-control-server failed-communication [endpoint:1] [setOrClear:1]
-
Simulate or clear a failed communication event on the barrier (i.e., set or clear the FailedCommunication bit in the SafetyStatus attribute).
- endpoint - INT8U - The endpoint on which to simulate this failed communication event
- setOrClear - INT8U - Whether to set (1) or clear (0) the failed communication state
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_OPEN |
plugin barrier-control-server open [endpoint:1]
-
Notify the plugin that the barrier has been opened manually.
- endpoint - INT8U - The endpoint on which the barrier has been opened
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_POSITION_FAILURE |
plugin barrier-control-server position-failure [endpoint:1] [setOrClear:1]
-
Simulate or clear a position failure event on the barrier (i.e., set or clear the PositionFailure bit in the SafetyStatus attribute).
- endpoint - INT8U - The endpoint on which to simulate this position failure event
- setOrClear - INT8U - Whether to set (1) or clear (0) the position failure state
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_REMOTE_LOCKOUT |
plugin barrier-control-server remote-lockout [endpoint:1] [setOrClear:1]
-
Simulate or clear a remote lockout event on the barrier (i.e., set or clear the RemoteLockout bit in the SafetyStatus attribute).
- endpoint - INT8U - The endpoint on which to simulate this remote lockout event
- setOrClear - INT8U - Whether to set (1) or clear (0) the remove lockout state
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_STATUS |
plugin barrier-control-server status [endpoint:1]
-
Prints out the status of the Barrier Control server cluster implementation.
- endpoint - INT8U - The endpoint from which to receive status
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BARRIER_CONTROL_SERVER_PLUGIN_BARRIER_CONTROL_SERVER_TAMPER_DETECTED |
plugin barrier-control-server tamper-detected [endpoint:1] [setOrClear:1]
-
Simulate or clear a tamper detected event on the barrier (i.e., set or clear the TamperDetected bit in the SafetyStatus attribute).
- endpoint - INT8U - The endpoint on which to simulate this tamper detected event
- setOrClear - INT8U - Whether to set (1) or clear (0) the tamper detected state