EmberAfOtaImageId Struct Reference
This is a unique identifier for referencing zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.
#include <
af-types.h
>
Data Fields |
|
| uint16_t | manufacturerId |
| uint16_t | imageTypeId |
| uint32_t | firmwareVersion |
| uint8_t | deviceSpecificFileEui64 [ EUI64_SIZE ] |
This is a unique identifier for referencing zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.
Field Documentation
| uint8_t EmberAfOtaImageId::deviceSpecificFileEui64[ EUI64_SIZE ] |
This is only used for device specific files. It will be set to all 0's when the image does not have an upgrade destination field in it. Little endian format.
| uint32_t EmberAfOtaImageId::firmwareVersion |
| uint16_t EmberAfOtaImageId::imageTypeId |
| uint16_t EmberAfOtaImageId::manufacturerId |
The documentation for this struct was generated from the following file:
-
af-types.h