Plugin Commands: Partner Link Key Exchange
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER |
|
plugin partner-link-key-exchange allow-partner [allowPartner:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER |
|
plugin partner-link-key-exchange partner [nodeId:2] [endpoint:1]
|
|
Detailed Description
The partner link key exchange plugin contributes CLI commands to the application framework to be used for controlling facets of link key exchanges among partners.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER |
plugin partner-link-key-exchange allow-partner [allowPartner:1]
-
Set the allow partner flag within the device for Certificate Based Key Exchange
- allowPartner - INT8U - Boolean value to allow or disallow partner based key exchange
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER |
plugin partner-link-key-exchange partner [nodeId:2] [endpoint:1]
-
Initiate partner link key exchange.
- nodeId - INT16U - The 2 byte short address of the node
- endpoint - INT8U - The endpoint of the device with whom ot start cbke.