EmberAfAttributeMinMaxValue Struct Reference
Type describing the attribute default, min and max values.
#include <
af-types.h
>
Data Fields |
|
| EmberAfDefaultAttributeValue | defaultValue |
| EmberAfDefaultAttributeValue | minValue |
| EmberAfDefaultAttributeValue | maxValue |
Type describing the attribute default, min and max values.
This struct is required if the attribute mask specifies that this attribute has a known min and max values.
Field Documentation
| EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::defaultValue |
Default value of the attribute.
| EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::maxValue |
Maximum allowed value.
| EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::minValue |
Minimum allowed value
The documentation for this struct was generated from the following file:
-
af-types.h