EmberZigbeeNetwork Struct Reference
Defines a ZigBee network and the associated parameters.
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | panId |
| uint8_t | channel |
| bool | allowingJoin |
| uint8_t | extendedPanId [ EXTENDED_PAN_ID_SIZE ] |
| uint8_t | stackProfile |
| uint8_t | nwkUpdateId |
Defines a ZigBee network and the associated parameters.
Field Documentation
| bool EmberZigbeeNetwork::allowingJoin |
| uint8_t EmberZigbeeNetwork::channel |
| uint8_t EmberZigbeeNetwork::extendedPanId[ EXTENDED_PAN_ID_SIZE ] |
| uint8_t EmberZigbeeNetwork::nwkUpdateId |
| uint16_t EmberZigbeeNetwork::panId |
| uint8_t EmberZigbeeNetwork::stackProfile |
The documentation for this struct was generated from the following file:
-
ember-types.h