Plugin Commands: Manufacturing Library CLI
Detailed Description
CLI commands related to the manufacturing library.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_MFGENABLE |
plugin mfglib mfgenable [enabled:1]
-
Enable mfglib.
- enabled - INT8U - 1 = enable, 0 = disable.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_PROGRAM_EUI |
plugin mfglib programEui [duration:8]
-
Program EUI.
- duration - IEEE_ADDRESS - IEEE address to program.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_MESSAGE |
plugin mfglib send message [data:-1] [numPackets:2]
-
Send a test message with the specified data in it.
- data - OCTET_STRING - The hex data to send, up to 16 bytes.
- numPackets - INT16U - The number of packets to send.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_RANDOM |
plugin mfglib send random [numPackets:2] [length:1]
-
Send a series of test packets with random data..
- numPackets - INT16U - The number of packets to send.
- length - INT8U - The length of the packet to send.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_TEST |
plugin mfglib send test [numPackets:2] [length:1]
-
Send a series of test packets with fixed data.
- numPackets - INT16U - The number of packets to send.
- length - INT8U - The length of the packet to send.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_CHANNEL |
plugin mfglib set-channel [channel:1]
-
Sets the channel used by the manufacturing library for testing.
- channel - INT8U - The 802.15.4 channel number.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_OPTIONS |
plugin mfglib set-options [options:1]
-
Sets options in the manufacturing library for testing.
- options - INT8U - The options bitmask (0 = normal transmit, 1 = CSMA transmit).
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_POWER |
plugin mfglib set-power [powerLevel:1] [powerMode:2]
-
Set the power level and mode for the manufacturing test.
- powerLevel - INT8S - The power level
- powerMode - INT16U - The power mode
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SLEEP |
plugin mfglib sleep [duration:2]
-
Sleep.
- duration - INT16U - Sleep duration (mS).
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_START |
plugin mfglib start [useCallback:1]
-
Start the mfglib test mode.
- useCallback - BOOLEAN - Use the Rx callback.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STATUS |
plugin mfglib status
- Prints the current status of the manufacturing library.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STOP |
plugin mfglib stop
- Stop the mfglib test mode.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_START |
plugin mfglib stream start
- Start the stream test.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_STOP |
plugin mfglib stream stop
- Stop the stream test.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_START |
plugin mfglib tone start
- Starts a tone test.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_STOP |
plugin mfglib tone stop
- Stops the tone test.