Plugin Commands: Address Table
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD |
|
plugin address-table add [entry:8]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP |
|
plugin address-table lookup [entry:8]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT |
|
plugin address-table print
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE |
|
plugin address-table remove [entry:8]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET |
|
plugin address-table set [index:1] [eui64:8] [nodeId:2]
|
|
Detailed Description
This plugin provides a set of APIs and CLI commands for managing the address table
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD |
plugin address-table add [entry:8]
-
Add an entry to the address table.
- entry - IEEE_ADDRESS - Entry to be added.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP |
plugin address-table lookup [entry:8]
-
Lookup an entry in the address table.
- entry - IEEE_ADDRESS - Entry to be looked up.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT |
plugin address-table print
- Prints the address table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE |
plugin address-table remove [entry:8]
-
Remove an entry from the address table.
- entry - IEEE_ADDRESS - Entry to be removed.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET |
plugin address-table set [index:1] [eui64:8] [nodeId:2]
-
Set an entry in the address table according to the arguments specified
- index - INT8U
- eui64 - IEEE_ADDRESS
- nodeId - INT16U