EmberAfStandaloneBootloaderQueryResponseData Struct Reference
A data struct for the information retrieved during a response to an Ember Bootloader over-the-air query.
#include <
af-types.h
>
Data Fields |
|
| uint8_t | hardwareTag [ EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH ] |
| uint8_t | eui64 [ EUI64_SIZE ] |
| uint16_t | mfgId |
| uint16_t | bootloaderVersion |
| uint8_t | capabilities |
| uint8_t | platform |
| uint8_t | micro |
| uint8_t | phy |
| bool | bootloaderActive |
A data struct for the information retrieved during a response to an Ember Bootloader over-the-air query.
Field Documentation
| bool EmberAfStandaloneBootloaderQueryResponseData::bootloaderActive |
| uint16_t EmberAfStandaloneBootloaderQueryResponseData::bootloaderVersion |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::capabilities |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::eui64[ EUI64_SIZE ] |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::hardwareTag[ EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH ] |
| uint16_t EmberAfStandaloneBootloaderQueryResponseData::mfgId |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::micro |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::phy |
| uint8_t EmberAfStandaloneBootloaderQueryResponseData::platform |
The documentation for this struct was generated from the following file:
-
af-types.h