Structure for ZCL command "QuerySpecificFileRequest" from "Over the Air Bootloading".

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

requestNodeAddress#

uint8_t* __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::requestNodeAddress

Definition at line 1964 of file app/zaptest/unit-test/zap-command-structs.h

manufacturerId#

uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::manufacturerId

Definition at line 1965 of file app/zaptest/unit-test/zap-command-structs.h

imageType#

uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::imageType

Definition at line 1966 of file app/zaptest/unit-test/zap-command-structs.h

fileVersion#

uint32_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::fileVersion

Definition at line 1967 of file app/zaptest/unit-test/zap-command-structs.h

currentZigbeeStackVersion#

uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::currentZigbeeStackVersion

Definition at line 1968 of file app/zaptest/unit-test/zap-command-structs.h