Cluster Commands: Basic
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_RTFD |
zcl basic rtfd | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLS |
zcl basic gls [startLocale:-1] [maxLocalesRequested:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLSR |
zcl basic glsr [discoveryComplete:1] [localeSupported:-1] |
Detailed Description
This group describes the CLI commands for the Basic cluster. Listed below is a description of the cluster:
Attributes for determining basic information about a device, setting user device information such as location, and enabling a device.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLS |
zcl basic gls [startLocale:-1] [maxLocalesRequested:1]
- This command gets locales supported.
- startLocale - CHAR_STRING
- maxLocalesRequested - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLSR |
zcl basic glsr [discoveryComplete:1] [localeSupported:-1]
- The locales supported response command is sent in response to a get locales supported command, and is used to discover which locales the device supports.
- discoveryComplete - INT8U
- localeSupported - CHAR_STRING
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_RTFD |
zcl basic rtfd
- Command that resets all attribute values to factory default.