Plugin Commands: Demand Response and Load Control
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR |
plugin drlc clear [endpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN |
plugin drlc opt in [endpoint:1] [eventId:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT |
plugin drlc opt out [endpoint:1] [eventId:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT |
plugin drlc print [endpoint:1] |
Detailed Description
The drlc plugin contributes CLI commands to the application framework to be used for constructing demand response load control commands.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR |
plugin drlc clear [endpoint:1]
- Clear the load control event table.
- endpoint - INT8U - The relevant endpoint.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN |
plugin drlc opt in [endpoint:1] [eventId:4]
- Modify the entry in the clients load control event table to opt in for a scheduled load control event.
- endpoint - INT8U - The relevant endpoint.
- eventId - INT32U - The event id of the event that the user is opting in or out of.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT |
plugin drlc opt out [endpoint:1] [eventId:4]
- Modify the entry in the clients load control event table to opt out of a scheduled load control event.
- endpoint - INT8U - The relevant endpoint.
- eventId - INT32U - The event id of the event that the user is opting in or out of.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT |
plugin drlc print [endpoint:1]
- Print the Demand Response Load Control Table.
- endpoint - INT8U - The relevant endpoint.