Cluster Commands: Generic Tunnel
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_MATCH |
zcl tunnel match [protocolAddress:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_RESPONSE |
zcl tunnel response [deviceIeeeAddress:8] [protocolAddress:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_ADVERTISE |
zcl tunnel advertise [protocolAddress:-1] |
Detailed Description
This group describes the CLI commands for the Generic Tunnel cluster. Listed below is a description of the cluster:
The minimum common commands and attributes required to tunnel any protocol.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_ADVERTISE |
zcl tunnel advertise [protocolAddress:-1]
- This command is typically sent upon startup, and whenever the ProtocolAddress attribute changes. It is typically multicast to a group of inter-communicating Generic Tunnel clusters.
- protocolAddress - OCTET_STRING
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_MATCH |
zcl tunnel match [protocolAddress:-1]
- This command is generated when an application wishes to find the ZigBee address (node, endpoint) of the Generic Tunnel server cluster with a given ProtocolAddress attribute. The command is typically multicast to a group of inter-communicating Generic Tunnel clusters
- protocolAddress - OCTET_STRING
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_RESPONSE |
zcl tunnel response [deviceIeeeAddress:8] [protocolAddress:-1]
- This command is generated upon receipt of a Match Protocol Address command to indicate that the Protocol Address was successfully matched.
- deviceIeeeAddress - IEEE_ADDRESS
- protocolAddress - OCTET_STRING