Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG
 plugin concentrator agg
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_HOST_TABLE
 plugin concentrator print-host-table
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE
 plugin concentrator print-table
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR
 plugin concentrator set-router-behavior [behavior:1]
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START
 plugin concentrator start
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS
 plugin concentrator status
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP
 plugin concentrator stop

Detailed Description

The Concentrator plugin contributes several CLI commands to the application framework for controlling the sending of MTORRs.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG

plugin concentrator agg

  • (Requires Concentrator Support to be enabled on this device.) Schedules a ZigBee PRO Many To One Route Request (MTORR) to be sent out at next opportunity, which will cause aggregation (many-to-one) routes to be created towards this concentrator.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_HOST_TABLE

plugin concentrator print-host-table

  • Print the host source route table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE

plugin concentrator print-table

  • Print the SOC/NCP source route table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR

plugin concentrator set-router-behavior [behavior:1]

  • This command allows the user to set the router behavior for this plugin. The argument values come from concentrator-support.h in the enum with members starting with EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_.
    • behavior - INT8U - The value of a EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_ enum member.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START

plugin concentrator start

  • Starts the periodic broadcast of MTORRs
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS

plugin concentrator status

  • Prints current status and configured parameters of the concentrator
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP

plugin concentrator stop

  • Stops the periodic broadcast of MTORRs