Cluster Commands: Prepayment
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SEL_AV_EM_CRED |
zcl prepayment sel-av-em-cred [commandIssueDateTime:4] [originatingDevice:1] [siteId:-1] [meterSerialNumber:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_DEBT |
zcl prepayment chg-debt [issuerEventId:4] [debtLabel:-1] [debtAmount:4] [debtRecoveryMethod:1] [debtAmountType:1] [debtRecoveryStartTime:4] [debtRecoveryCollectionTime:2] [debtRecoveryFrequency:1] [debtRecoveryAmount:4] [debtRecoveryBalancePercentage:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_EM_CRED_SETUP |
zcl prepayment em-cred-setup [issuerEventId:4] [startTime:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP |
zcl prepayment cons-top-up [originatingDevice:1] [topUpCode:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CRED_ADJ |
zcl prepayment cred-adj [issuerEventId:4] [startTime:4] [creditAdjustmentType:1] [creditAdjustmentValue:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE |
zcl prepayment chg-pmt-mode [providerId:4] [issuerEventId:4] [implementationDateTime:4] [proposedPaymentControlConfiguration:2] [cutOffValue:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_PP_SS |
zcl prepayment get-pp-ss [earliestStartTime:4] [latestEndTime:4] [snapshotOffset:1] [snapshotCause:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_TOP_UP_LOG |
zcl prepayment get-top-up-log [latestEndTime:4] [numberOfRecords:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_LOW_CRED_WNG_LVL |
zcl prepayment set-low-cred-wng-lvl [lowCreditWarningLevel:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_DEBT_REPMT_LOG |
zcl prepayment get-debt-repmt-log [latestEndTime:4] [numberOfDebts:1] [debtType:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_MAX_CRED_LMT |
zcl prepayment set-max-cred-lmt [providerId:4] [issuerEventId:4] [implementationDateTime:4] [maximumCreditLevel:4] [maximumCreditPerTopUp:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_OA_DEBT_CAP |
zcl prepayment set-oa-debt-cap [providerId:4] [issuerEventId:4] [implementationDateTime:4] [overallDebtCap:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_PREP_SS |
zcl prepayment pub-prep-ss [snapshotId:4] [snapshotTime:4] [totalSnapshotsFound:1] [commandIndex:1] [totalNumberOfCommands:1] [snapshotCause:4] [snapshotPayloadType:1] [snapshotPayload:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE_RESP |
zcl prepayment chg-pmt-mode-resp [friendlyCredit:1] [friendlyCreditCalendarId:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP_RESP |
zcl prepayment cons-top-up-resp [resultType:1] [topUpValue:4] [sourceOfTopUp:1] [creditRemaining:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_TOP_UP_LOG |
zcl prepayment pub-top-up-log [commandIndex:1] [totalNumberOfCommands:1] [topUpPayload:7] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_DEBT_LOG |
zcl prepayment pub-debt-log [commandIndex:1] [totalNumberOfCommands:1] [debtPayload:13] |
Detailed Description
This group describes the CLI commands for the Prepayment cluster. Listed below is a description of the cluster:
The Prepayment Cluster provides the facility to pass messages relating to prepayment between devices on the HAN.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_DEBT |
zcl prepayment chg-debt [issuerEventId:4] [debtLabel:-1] [debtAmount:4] [debtRecoveryMethod:1] [debtAmountType:1] [debtRecoveryStartTime:4] [debtRecoveryCollectionTime:2] [debtRecoveryFrequency:1] [debtRecoveryAmount:4] [debtRecoveryBalancePercentage:2]
- The ChangeDebt command is send to the Metering Device to change the fuel or Non fuel debt values.
- issuerEventId - INT32U
- debtLabel - OCTET_STRING
- debtAmount - INT32U
- debtRecoveryMethod - DebtRecoveryMethod [ENUM8]
- debtAmountType - DebtAmountType [ENUM8]
- debtRecoveryStartTime - UTC_TIME
- debtRecoveryCollectionTime - INT16U
- debtRecoveryFrequency - DebtRecoveryFrequency [ENUM8]
- debtRecoveryAmount - INT32U
- debtRecoveryBalancePercentage - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE |
zcl prepayment chg-pmt-mode [providerId:4] [issuerEventId:4] [implementationDateTime:4] [proposedPaymentControlConfiguration:2] [cutOffValue:4]
- This command is sent to a Metering Device to instruct it to change its mode of operation. i.e. from Credit to Prepayment.
- providerId - INT32U
- issuerEventId - INT32U
- implementationDateTime - UTC_TIME
- proposedPaymentControlConfiguration - PaymentControlConfiguration [BITMAP16]
- cutOffValue - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CHG_PMT_MODE_RESP |
zcl prepayment chg-pmt-mode-resp [friendlyCredit:1] [friendlyCreditCalendarId:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
- This command is send in response to the ChangePaymentMode Command.
- friendlyCredit - FriendlyCredit [BITMAP8]
- friendlyCreditCalendarId - INT32U
- emergencyCreditLimit - INT32U
- emergencyCreditThreshold - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP |
zcl prepayment cons-top-up [originatingDevice:1] [topUpCode:-1]
- The ConsumerTopUp command is used by the IPD and the ESI as a method of applying credit top up values to the prepayment meter.
- originatingDevice - OriginatingDevice [ENUM8]
- topUpCode - OCTET_STRING
- See also
- EmberAfOriginatingDevice
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CONS_TOP_UP_RESP |
zcl prepayment cons-top-up-resp [resultType:1] [topUpValue:4] [sourceOfTopUp:1] [creditRemaining:4]
- This command is send in response to the ConsumerTopUp Command.
- resultType - ResultType [ENUM8]
- topUpValue - INT32U
- sourceOfTopUp - OriginatingDevice [ENUM8]
- creditRemaining - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_CRED_ADJ |
zcl prepayment cred-adj [issuerEventId:4] [startTime:4] [creditAdjustmentType:1] [creditAdjustmentValue:4]
- The CreditAdjustment command is sent to update the accounting base for the Prepayment meter.
- issuerEventId - INT32U
- startTime - UTC_TIME
- creditAdjustmentType - CreditAdjustmentType [ENUM8]
- creditAdjustmentValue - INT32U
- See also
- EmberAfCreditAdjustmentType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_EM_CRED_SETUP |
zcl prepayment em-cred-setup [issuerEventId:4] [startTime:4] [emergencyCreditLimit:4] [emergencyCreditThreshold:4]
- This command is a method to set up the parameters for the emergency credit.
- issuerEventId - INT32U
- startTime - UTC_TIME
- emergencyCreditLimit - INT32U
- emergencyCreditThreshold - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_DEBT_REPMT_LOG |
zcl prepayment get-debt-repmt-log [latestEndTime:4] [numberOfDebts:1] [debtType:1]
- This command is used to request the contents of the repayment log.
- latestEndTime - UTC_TIME
- numberOfDebts - INT8U
- debtType - RepaymentDebtType [ENUM8]
- See also
- EmberAfRepaymentDebtType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_PP_SS |
zcl prepayment get-pp-ss [earliestStartTime:4] [latestEndTime:4] [snapshotOffset:1] [snapshotCause:4]
- This command is used to request the cluster server for snapshot data.
- earliestStartTime - UTC_TIME
- latestEndTime - UTC_TIME
- snapshotOffset - INT8U
- snapshotCause - PrepaySnapshotPayloadCause [BITMAP32]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_GET_TOP_UP_LOG |
zcl prepayment get-top-up-log [latestEndTime:4] [numberOfRecords:1]
- This command is sent to the Metering Device to retrieve the log of Top Up codes received by the meter.
- latestEndTime - UTC_TIME
- numberOfRecords - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_DEBT_LOG |
zcl prepayment pub-debt-log [commandIndex:1] [totalNumberOfCommands:1] [debtPayload:13]
- This command is used to send the contents of the Repayment Log.
- commandIndex - INT8U
- totalNumberOfCommands - INT8U
- debtPayload - struct DebtPayload
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_PREP_SS |
zcl prepayment pub-prep-ss [snapshotId:4] [snapshotTime:4] [totalSnapshotsFound:1] [commandIndex:1] [totalNumberOfCommands:1] [snapshotCause:4] [snapshotPayloadType:1] [snapshotPayload:1]
- This command is generated in response to a GetPrepaySnapshot command. It is used to return a single snapshot to the client.
- snapshotId - INT32U
- snapshotTime - UTC_TIME
- totalSnapshotsFound - INT8U
- commandIndex - INT8U
- totalNumberOfCommands - INT8U
- snapshotCause - PrepaySnapshotPayloadCause [BITMAP32]
- snapshotPayloadType - PrepaySnapshotPayloadType [ENUM8]
- snapshotPayload - INT8U
- See also
- EmberAfPrepaySnapshotPayloadType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_PUB_TOP_UP_LOG |
zcl prepayment pub-top-up-log [commandIndex:1] [totalNumberOfCommands:1] [topUpPayload:7]
- This command is used to send the Top Up Code Log entries to the client.
- commandIndex - INT8U
- totalNumberOfCommands - INT8U
- topUpPayload - struct TopUpPayload
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SEL_AV_EM_CRED |
zcl prepayment sel-av-em-cred [commandIssueDateTime:4] [originatingDevice:1] [siteId:-1] [meterSerialNumber:-1]
- This command is sent to the Metering Device to activate the use of any Emergency Credit available on the Metering Device.
- commandIssueDateTime - UTC_TIME
- originatingDevice - OriginatingDevice [ENUM8]
- siteId - OCTET_STRING
- meterSerialNumber - OCTET_STRING
- See also
- EmberAfOriginatingDevice
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_LOW_CRED_WNG_LVL |
zcl prepayment set-low-cred-wng-lvl [lowCreditWarningLevel:4]
- This command is sent from client to a Prepayment server to set the warning level for low credit.
- lowCreditWarningLevel - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_MAX_CRED_LMT |
zcl prepayment set-max-cred-lmt [providerId:4] [issuerEventId:4] [implementationDateTime:4] [maximumCreditLevel:4] [maximumCreditPerTopUp:4]
- This command is sent from a client to the Prepayment server to set the maximum credit level allowed in the meter.
- providerId - INT32U
- issuerEventId - INT32U
- implementationDateTime - UTC_TIME
- maximumCreditLevel - INT32U
- maximumCreditPerTopUp - INT32U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PREPAYMENT_SET_OA_DEBT_CAP |
zcl prepayment set-oa-debt-cap [providerId:4] [issuerEventId:4] [implementationDateTime:4] [overallDebtCap:4]
- This command is sent from a client to the Prepayment server to set the overall debt cap allowed in the meter.
- providerId - INT32U
- issuerEventId - INT32U
- implementationDateTime - UTC_TIME
- overallDebtCap - INT32U