Plugin Commands: Relay Control Server
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_GET |
plugin relay-control-server get [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_SET |
plugin relay-control-server set [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [isEnabled:1] |
Detailed Description
The relay control plugin provides the functionality to enable or disable the stack's relay capabilities, and also to view the relay state.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_GET |
plugin relay-control-server get [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
- Get the relay state
- nodeId - INT16U - the destination node id
- srcEndpoint - INT8U - the source endpoint
- dstEndpoint - INT8U - the destination endpoint
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_SET |
plugin relay-control-server set [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [isEnabled:1]
- Set the relay state
- nodeId - INT16U - the destination node id
- srcEndpoint - INT8U - the source endpoint
- dstEndpoint - INT8U - the destination endpoint
- isEnabled - INT8U - state value to be set