EmberAfMessageStruct Struct Reference
The EmberAfMessageStruct is a struct wrapper that contains all the data about a low-level message to be sent (it may be ZCL or may be some other protocol).
#include <
af-types.h
>
Data Fields | |
EmberAfMessageSentFunction | callback |
EmberApsFrame * | apsFrame |
uint8_t * | message |
uint16_t | indexOrDestination |
uint16_t | messageLength |
EmberOutgoingMessageType | type |
bool | broadcast |
The EmberAfMessageStruct is a struct wrapper that contains all the data about a low-level message to be sent (it may be ZCL or may be some other protocol).
Field Documentation
EmberApsFrame* EmberAfMessageStruct::apsFrame |
bool EmberAfMessageStruct::broadcast |
EmberAfMessageSentFunction EmberAfMessageStruct::callback |
uint16_t EmberAfMessageStruct::indexOrDestination |
uint8_t* EmberAfMessageStruct::message |
uint16_t EmberAfMessageStruct::messageLength |
EmberOutgoingMessageType EmberAfMessageStruct::type |
The documentation for this struct was generated from the following file:
af-types.h