Plugin Commands: Device Table
Detailed Description
The device table plugin demonstrates tracking devices as they join the
gateway's ZigBee network.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_CLEAR |
plugin device-table clear
- Clear the device table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_DISC |
plugin device-table disc [nodeId:2]
- Force a (re)discovery of the device based on the node ID.
- nodeId - INT16U - Node ID to discover.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREMOVE |
plugin device-table iremove [index:2]
- Remove device from device table.
- index - INT16U - Device table index.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREPAIR |
plugin device-table irepair [index:2]
- Kick off device route repair.
- index - INT16U - Device table index.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_ISEND |
plugin device-table isend [index:2]
- Send to device in device table.
- index - INT16U - Device table index.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LEAVE |
plugin device-table leave [eui64:8]
- Remove device from device table.
- eui64 - IEEE_ADDRESS - EUI64 of device.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LOAD |
plugin device-table load
- Load the file.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_PRINT |
plugin device-table print
- Print the device table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REMOVE |
plugin device-table remove [eui64:8]
- Remove device from device table.
- eui64 - IEEE_ADDRESS - EUI64 of device.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REPAIR |
plugin device-table repair [eui64:8]
- Kick off device route repair.
- eui64 - IEEE_ADDRESS - EUI64 of device.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SAVE |
plugin device-table save
- Save the file.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SEND |
plugin device-table send [eui64:8] [endpoint:1]
- Send to device in device table.
- eui64 - IEEE_ADDRESS - EUI64 of device.
- endpoint - INT8U - Endpoint of device.