EmberAfTimeStruct Struct Reference
A data structure used to describe the time in a human understandable format (as opposed to 32-bit UTC)
#include <
af-types.h
>
Data Fields | |
uint16_t | year |
uint8_t | month |
uint8_t | day |
uint8_t | hours |
uint8_t | minutes |
uint8_t | seconds |
A data structure used to describe the time in a human understandable format (as opposed to 32-bit UTC)
Field Documentation
uint8_t EmberAfTimeStruct::day |
uint8_t EmberAfTimeStruct::hours |
uint8_t EmberAfTimeStruct::minutes |
uint8_t EmberAfTimeStruct::month |
uint8_t EmberAfTimeStruct::seconds |
uint16_t EmberAfTimeStruct::year |
The documentation for this struct was generated from the following file:
af-types.h