Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_BACKOFF_CONFIG
plugin ias-zone-server change-backoff-config [firstBackoff:1] [commonRatio:1] [maxBackoff:4] [unlimitedRetries:1] [maxRetryAttempts:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_STATUS
plugin ias-zone-server changeStatus [newStatus:2] [timeSinceOccurredSeconds:1] [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_INFO
plugin ias-zone-server info [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE
plugin ias-zone-server print-queue
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE_CONFIG
plugin ias-zone-server print-queue-config
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_SET_ENROLLMENT_MODE
plugin ias-zone-server set-enrollment-mode [endpoint:1] [enrollmentMode:1]

Detailed Description

This plugin provides a set of CLI commands for managing the local IAS Zone server.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_BACKOFF_CONFIG

plugin ias-zone-server change-backoff-config [firstBackoff:1] [commonRatio:1] [maxBackoff:4] [unlimitedRetries:1] [maxRetryAttempts:2]

  • Update the IAS Zone server's backoff configuration parameters.
    • firstBackoff - INT8U - First backoff time in seconds.
    • commonRatio - INT8U - Backoff increase common ratio.
    • maxBackoff - INT32U - Maximum backoff time in seconds.
    • unlimitedRetries - BOOLEAN - Unlimited retires.
    • maxRetryAttempts - INT16U - Maximum retry attempts.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_STATUS

plugin ias-zone-server changeStatus [newStatus:2] [timeSinceOccurredSeconds:1] [endpoint:1]

  • Update the zone status attribute of a given endpoint's IAS Zone cluster to the given value
    • newStatus - INT16U - The new status to be written
    • timeSinceOccurredSeconds - INT8U - The amount time that has passed since the last update occurred (seconds)
    • endpoint - INT8U - The endpoint whose zone status attribute is to be updated
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_INFO

plugin ias-zone-server info [endpoint:1]

  • Print current value of the following cluster attributes: zone type, zone state, zone status, zone id
    • endpoint - INT8U - The endpoint whose IAS Zone Cluster information is to be printed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE

plugin ias-zone-server print-queue

  • Prints information on the status queue.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE_CONFIG

plugin ias-zone-server print-queue-config

  • Prints the status queue config.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_SET_ENROLLMENT_MODE

plugin ias-zone-server set-enrollment-mode [endpoint:1] [enrollmentMode:1]

  • Update the IAS Zone server's enrollment method to the specified value
    • endpoint - INT8U - The endpoint whose enrollment mode is to be updated
    • enrollmentMode - INT8U - The new enrollment mode