This structure contains information about a tag that resides within an Over-the-air bootload file.

#include <af-types.h>

Data Fields

uint16_t id
 
uint32_t length

This structure contains information about a tag that resides within an Over-the-air bootload file.

Field Documentation

uint16_t EmberAfTagData::id
uint32_t EmberAfTagData::length

The documentation for this struct was generated from the following file:
  • af-types.h