EmberAfPluginMessagingClientMessage Struct Reference

#include <af-types.h>

Data Fields

bool valid
 
bool active
 
EmberAfPluginEsiManagementBitmask esiBitmask
 
uint8_t clientEndpoint
 
uint32_t messageId
 
uint8_t messageControl
 
uint32_t startTime
 
uint32_t endTime
 
uint16_t durationInMinutes
 
uint8_t message [EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1]

Field Documentation

bool EmberAfPluginMessagingClientMessage::active
uint8_t EmberAfPluginMessagingClientMessage::clientEndpoint
uint16_t EmberAfPluginMessagingClientMessage::durationInMinutes
uint32_t EmberAfPluginMessagingClientMessage::endTime
EmberAfPluginEsiManagementBitmask EmberAfPluginMessagingClientMessage::esiBitmask
uint8_t EmberAfPluginMessagingClientMessage::message[EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1]
uint8_t EmberAfPluginMessagingClientMessage::messageControl
uint32_t EmberAfPluginMessagingClientMessage::messageId
uint32_t EmberAfPluginMessagingClientMessage::startTime
bool EmberAfPluginMessagingClientMessage::valid

The documentation for this struct was generated from the following file:
  • af-types.h