Plugin Commands: Standalone Bootloader Server
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_BOOTLOAD_EUI |
plugin standalone-bootloader-server bootload eui [eui64:8] [index:1] [tag:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_BOOTLOAD_TARGET |
plugin standalone-bootloader-server bootload target [index:1] [tag:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PRINT_TARGET |
plugin standalone-bootloader-server print-target | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_QUERY |
plugin standalone-bootloader-server query | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_STATUS |
plugin standalone-bootloader-server status |
Detailed Description
The Standalone Bootloader Server contributes commands to tell client's to launch their standalone bootloader and send them a new application image.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_BOOTLOAD_EUI |
plugin standalone-bootloader-server bootload eui [eui64:8] [index:1] [tag:1]
- Starts the process for bootloading a device using the passed EUI64.
- eui64 - IEEE_ADDRESS - The EUI64 of the target of the bootload.
- index - INT8U - The index of the image being sent to the target
- tag - INT8U - The tag ID within the image, which will be sent to the target.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_BOOTLOAD_TARGET |
plugin standalone-bootloader-server bootload target [index:1] [tag:1]
- Starts the process for bootloading a device using the currently cached target info.
- index - INT8U - The index of the image being sent to the target
- tag - INT8U - The tag ID within the image, which will be sent to the target.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PRINT_TARGET |
plugin standalone-bootloader-server print-target
- Print the cached info about the current bootload target.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_QUERY |
plugin standalone-bootloader-server query
n
Send a broadcast standalone bootloader query to all nearby nodes.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_STANDALONE_BOOTLOADER_SERVER_PLUGIN_STANDALONE_BOOTLOADER_SERVER_STATUS |
plugin standalone-bootloader-server status
- Print the standalone bootload server's current status.