EmberAfDefinedEndpoint Struct Reference
Struct that maps actual endpoint type, onto a specific endpoint.
#include <
af-types.h
>
Data Fields | |
uint8_t | endpoint |
EmberAfProfileId | profileId |
uint16_t | deviceId |
uint8_t | deviceVersion |
EmberAfEndpointType * | endpointType |
uint8_t | networkIndex |
EmberAfEndpointBitmask | bitmask |
Struct that maps actual endpoint type, onto a specific endpoint.
Field Documentation
EmberAfEndpointBitmask EmberAfDefinedEndpoint::bitmask |
Meta-data about the endpoint
uint16_t EmberAfDefinedEndpoint::deviceId |
Device ID of the device on this endpoint.
uint8_t EmberAfDefinedEndpoint::deviceVersion |
Version of the device.
uint8_t EmberAfDefinedEndpoint::endpoint |
Actual zigbee endpoint number.
EmberAfEndpointType* EmberAfDefinedEndpoint::endpointType |
Endpoint type for this endpoint.
uint8_t EmberAfDefinedEndpoint::networkIndex |
Network index for this endpoint.
EmberAfProfileId EmberAfDefinedEndpoint::profileId |
Profile ID of the device on this endpoint.
The documentation for this struct was generated from the following file:
af-types.h