EmberAfRemoteClusterStruct Struct Reference
Zigbee Internet Client/Server remote cluster struct.
#include <
af-types.h
>
Data Fields | |
EmberAfClusterId | clusterId |
EmberAfProfileId | profileId |
uint16_t | deviceId |
uint8_t | endpoint |
EmberAfRemoteClusterType | type |
Zigbee Internet Client/Server remote cluster struct.
Field Documentation
EmberAfClusterId EmberAfRemoteClusterStruct::clusterId |
uint16_t EmberAfRemoteClusterStruct::deviceId |
uint8_t EmberAfRemoteClusterStruct::endpoint |
EmberAfProfileId EmberAfRemoteClusterStruct::profileId |
EmberAfRemoteClusterType EmberAfRemoteClusterStruct::type |
The documentation for this struct was generated from the following file:
af-types.h