XNCP Library Callbacks
Functions | |
EmberStatus | emberAfPluginXncpIncomingCustomFrameCallback (uint8_t messageLength, uint8_t *messagePayload, uint8_t *replyPayloadLength, uint8_t *replyPayload) |
Called when the NCP receives a custom EZSP message from the HOST. | |
bool | emberAfIncomingMessageCallback (EmberIncomingMessageType type, EmberApsFrame *apsFrame, EmberMessageBuffer message) |
Called when the NCP receives an incoming Zigbee PRO message. | |
bool | emberAfPluginCommandHandlerPermitNcpToHostFrameCallback (uint8_t frameId, uint8_t payloadLength, uint8_t *payload) |
Called when the NCP wants to inform the HOST of a callback that has been called on the NCP. | |
bool | emberAfPluginCommandHandlerPermitHostToNcpFrameCallback (uint8_t frameId, uint8_t payloadLength, uint8_t *payload) |
Enables or disables the processing of EZSP commands on the NCP. | |
void | emberAfPluginXncpGetXncpInformation (uint16_t *manufacturerId, uint16_t *versionNumber) |
Gets XNCP information. |
Detailed Description
These callbacks are contributed by the XNCP Library plugin.
Function Documentation
bool emberAfIncomingMessageCallback | ( | EmberIncomingMessageType | type, |
EmberApsFrame * | apsFrame, |
||
EmberMessageBuffer | message |
||
) |
Called when the NCP receives an incoming Zigbee PRO message.
This handling is done before any other action is taken by the NCP on the callback. If the function returns true, the incoming message is done being handled, and the NCP does not need to record the callback or report it to the HOST.
- Parameters
-
type
The EmberIncomingMessageType of the incoming message. Ver.: always apsFrame
The EmberApsFrame recieved in the incoming message. Ver.: always message
The payload of the incoming message, in the form of an EmberMessageBuffer. Ver.: always
- Returns
- A ::bool value. If this value is true, the NCP will not handle the incoming message any further and it will not report the incoming message to the HOST. If the returned value is false, the NCP will continue to process the incoming message and the callback will also be passed to the HOST.
bool emberAfPluginCommandHandlerPermitHostToNcpFrameCallback | ( | uint8_t | frameId, |
uint8_t | payloadLength, |
||
uint8_t * | payload |
||
) |
Enables or disables the processing of EZSP commands on the NCP.
The application can use this callback to enable or disable the processing of EZSP commands on the NCP. If this function returns true, the frame will be handled by the NCP in a normal manner. If this function returns false, the NCP will disregard this command and respond to the HOST that it is an invalid frame.
- Parameters
-
frameId
The EZSP frame ID of the message. Ver.: always payloadLength
The length of the payload of the EZSP message. Ver.: always payload
The EZSP message payload. Ver.: always
- Returns
- A ::bool value indicating whether or not the frame will continue to be handled. If this function returns true, the frame will be handled by the NCP in a normal manner. If this function returns false, then the NCP will disregard this command and respond to the HOST that it is an invalid frame.
bool emberAfPluginCommandHandlerPermitNcpToHostFrameCallback | ( | uint8_t | frameId, |
uint8_t | payloadLength, |
||
uint8_t * | payload |
||
) |
Called when the NCP wants to inform the HOST of a callback that has been called on the NCP.
If this function returns false, the NCP will not notify the HOST of the callback. If the function returns true, then the NCP will continue scheduling the notification of the HOST regarding the callback.
- Parameters
-
frameId
The frameId of the callback. Ver.: always payloadLength
The length of the payload carried in the callback. Ver.: always payload
The actual payload carried by the callback. Ver.: always
- Returns
- A ::bool value. If the value is false, then the NCP will not notify the HOST of the callback. If the return value is true, the NCP will continue scheduling the notification of the HOST regarding the callback.
void emberAfPluginXncpGetXncpInformation | ( | uint16_t * | manufacturerId, |
uint16_t * | versionNumber |
||
) |
Gets XNCP information.
This callback enables users to communicate the version number and manufacturer ID of their NCP application to the framework. This information is needed for the EZSP command frame called getXncpInfo. This callback will be called when that frame is received so that the application can report its version number and manufacturer ID to be sent back to the HOST.
- Parameters
-
versionNumber
The version number of the NCP application. manufacturerId
The manufacturer ID of the NCP application.
EmberStatus emberAfPluginXncpIncomingCustomFrameCallback | ( | uint8_t | messageLength, |
uint8_t * | messagePayload, |
||
uint8_t * | replyPayloadLength, |
||
uint8_t * | replyPayload |
||
) |
Called when the NCP receives a custom EZSP message from the HOST.
The message length and payload is passed to the callback in the first two arguments. The implementation can then fill in the replyPayload and set the replayPayloadLength to the number of bytes in the replyPayload. See documentation for the function ezspCustomFrame on sending these messages from the HOST.
- Parameters
-
messageLength
The length of the messagePayload. messagePayload
The custom message that was sent from the HOST. Ver.: always replyPayloadLength
The length of the replyPayload. This needs to be set by the implementation for a properly formed response to be sent back to the HOST. Ver.: always replyPayload
The custom message to send back to the HOST in respose to the custom message. Ver.: always
- Returns
- An EmberStatus indicating the result of the custom message handling. This returned status is always the first byte of the EZSP response.
References EMBER_LIBRARY_NOT_PRESENT.