Plugin Commands: Compact Logger
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_CLEAR |
plugin compact-logger clear | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_FACILITY |
plugin compact-logger set-facility [facility:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_SEVERITY |
plugin compact-logger set-severity [severity:1] |
Detailed Description
The compact-logger plugin contributes CLI commands to the application framework to be used for storing information.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_CLEAR |
plugin compact-logger clear
- Clear the log
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_FACILITY |
plugin compact-logger set-facility [facility:2]
- Set the facility values messages must meet in order to be logged
- facility - INT16U - The new facility value.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_SEVERITY |
plugin compact-logger set-severity [severity:1]
- Sets the minimum severity level messages must meet in order to be logged
- severity - INT8U - The new severity level.