Plugin Commands: Sub-GHz Client
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS |
plugin sub-ghz get-suspend-status [nodeId:2] [ep:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS |
plugin sub-ghz ignore-suspend-status [ignore:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE |
plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1] |
Detailed Description
The Sub-GHz commands provide commands for sub-GHz duty cycle, power management and frequency agility.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS |
plugin sub-ghz get-suspend-status [nodeId:2] [ep:1]
- Send the GetSuspendZCLMessagesStatus command to the Sub-GHz server.
- nodeId - INT16U - Server's node ID
- ep - INT8U - Server's endpoint
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS |
plugin sub-ghz ignore-suspend-status [ignore:1]
- Ignore the suspend status when sending ZCL messages (for testing purposes only).
- ignore - BOOLEAN - Whether or not the suspend status should be ignored
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE |
plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1]
- Send the Mgmt_NWK_Unsolicited_Enhanced_Update_notify command to the Sub-GHz server.
- nodeId - INT16U - Server's node ID
- page - INT8U - Current channel page
- channel - INT8U - Current channel
- macTxUcastTotal - INT16U - Total number of Mac Tx transaction attempts
- macTxUcastFailures - INT16U - Total number of Mac Tx transaction failures
- macTxUcastRetries - INT16U - Total number of Mac Tx transaction retries
- period - INT8U - Time in minutes over which the Mac Tx counts were measured