EmberAfPluginReportingEntry Struct Reference
A structure used to store reporting configurations. If endpoint field is EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID, the entry is unused.
#include <
af-types.h
>
Data Fields | |
EmberAfReportingDirection | direction |
uint8_t | endpoint |
EmberAfClusterId | clusterId |
EmberAfAttributeId | attributeId |
uint8_t | mask |
uint16_t | manufacturerCode |
union { | |
struct { | |
uint16_t minInterval | |
uint16_t maxInterval | |
uint32_t reportableChange | |
} reported | |
struct { | |
EmberNodeId source | |
uint8_t endpoint | |
uint16_t timeout | |
} received | |
} | data |
A structure used to store reporting configurations. If endpoint field is EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID, the entry is unused.
Field Documentation
EmberAfAttributeId EmberAfPluginReportingEntry::attributeId |
The id of the attribute being reported or received.
EmberAfClusterId EmberAfPluginReportingEntry::clusterId |
The cluster where the attribute is located.
union { ... } EmberAfPluginReportingEntry::data |
EmberAfReportingDirection EmberAfPluginReportingEntry::direction |
EMBER_ZCL_REPORTING_DIRECTION_REPORTED for reports sent from the local device or EMBER_ZCL_REPORTING_DIRECTION_RECEIVED for reports received from a remote device.
uint8_t EmberAfPluginReportingEntry::endpoint |
The local endpoint from which the attribute is reported or to which the report is received. If EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID, the entry is unused.
The remote endpoint from which the attribute is reported.
uint16_t EmberAfPluginReportingEntry::manufacturerCode |
Manufacturer code associated with the cluster and/or attribute. If the cluster id is inside the manufacturer-specific range, this value indicates the manufacturer code for the cluster. Otherwise, if this value is non-zero and the cluster id is a standard ZCL cluster, it indicates the manufacturer code for attribute.
uint8_t EmberAfPluginReportingEntry::mask |
CLUSTER_MASK_SERVER for server-side attributes or CLUSTER_MASK_CLIENT for client-side attributes.
uint16_t EmberAfPluginReportingEntry::maxInterval |
The maximum reporting interval, measured in seconds.
uint16_t EmberAfPluginReportingEntry::minInterval |
The minimum reporting interval, measured in seconds.
struct { ... } EmberAfPluginReportingEntry::received |
uint32_t EmberAfPluginReportingEntry::reportableChange |
The minimum change to the attribute that will result in a report being sent.
struct { ... } EmberAfPluginReportingEntry::reported |
EmberNodeId EmberAfPluginReportingEntry::source |
The node id of the source of the received reports.
uint16_t EmberAfPluginReportingEntry::timeout |
The maximum expected time between reports, measured in seconds.
The documentation for this struct was generated from the following file:
af-types.h