#include <af-types.h
>
uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::divisor |
uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::measurementPeriod |
uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::multiplier |
uint8_t EmberAfDeviceManagementUncontrolledFlowThreshold::stabilisationPeriod |
uint16_t EmberAfDeviceManagementUncontrolledFlowThreshold::uncontrolledFlowThreshold |
uint8_t EmberAfDeviceManagementUncontrolledFlowThreshold::unitOfMeasure |
The documentation for this struct was generated from the following file: