EmberAfStandaloneBootloaderQueryResponseData Struct Reference
A data struct for the information retrieved during a response to an Ember Bootloader over-the-air query.
#include <
af-types.h
>
Data Fields | |
uint8_t | hardwareTag [EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH] |
uint8_t | eui64 [EUI64_SIZE] |
uint16_t | mfgId |
uint16_t | bootloaderVersion |
uint8_t | capabilities |
uint8_t | platform |
uint8_t | micro |
uint8_t | phy |
bool | bootloaderActive |
A data struct for the information retrieved during a response to an Ember Bootloader over-the-air query.
Field Documentation
bool EmberAfStandaloneBootloaderQueryResponseData::bootloaderActive |
uint16_t EmberAfStandaloneBootloaderQueryResponseData::bootloaderVersion |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::capabilities |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::eui64[EUI64_SIZE] |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::hardwareTag[EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH] |
uint16_t EmberAfStandaloneBootloaderQueryResponseData::mfgId |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::micro |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::phy |
uint8_t EmberAfStandaloneBootloaderQueryResponseData::platform |
The documentation for this struct was generated from the following file:
af-types.h