Detailed Description
The Security command set includes all of the commands related to security configuration on the device.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI__SECURITY_MFG_TOKEN_COMMANDS |
Commands used for security.
security mfg-token get security mfg-token set <Magic number> <EmberKeySettings value>
- Magic number - uint32_t. The 4-byte magic number EMBER_MFG_SECURITY_CONFIG_MAGIC_NUMBER to prevent accidental execution.
- EmberKeySettings value - uint16_t. The 2-byte value for EmberKeySettings indicating key permissions.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_LINK |
changekey link [key:-1]
- Change the link key to the one provided in the 16 byte array argument for this command.
- key - OCTET_STRING - The link key provided as a 16 byte array
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_NETWORK |
changekey network [key:-1]
- Change the network key to the 16 byte array provided as an argument to this command.
- key - OCTET_STRING - The network key provided as a 16 byte array
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_CLEAR |
keys clear
- Clear all security keys
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_DELETE |
keys delete [index:1]
- Delete a security key from a given index
- index - INT8U - index into the security key table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_PRINT |
keys print
- Print all security keys out to the command line.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_INSTALL_CODE |
option install-code [keyTableIndex:1] [ieeeAddress:8] [installCode:-1]
- Derives a link key from an install code and sets it in the link key table.
- keyTableIndex - INT8U - index into the link key table
- ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
- installCode - OCTET_STRING - install code including two-byte, little-endian CRC
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_LINK |
option link [keyTableIndex:1] [ieeeAddress:8] [linkKey:-1]
- Sets a link key in the link key table. Example: option link 0x00 { 06 00 ab 41 64 30 00 0a } {aa bb cc dd ee ff aa bb cc dd ee ff aa bb cc dd}
- keyTableIndex - INT8U - index into the link key table
- ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
- linkKey - OCTET_STRING - link key to enter into the table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_REGISTER |
option register
- Initiates Smart Energy Registration including Key Establishment. This command expects that the device has already joined a smart energy network.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_OFF |
option security aps off
- Turns aps security off
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_ON |
option security aps on
- Turns aps security on
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY |
option security set-allow-trust-center-rejoin-using-well-known-key [allowTrustCenterRejoinUsingWellKnownKey:1]
- Set whether or not a Trust Center application will allow trust center rejoins for devices using the well-known key.
- allowTrustCenterRejoinUsingWellKnownKey - BOOLEAN - Whether or not the Trust Center should allow trust center rejoins for devices using the well-known key.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY_TIMEOUT |
option security set-allow-trust-center-rejoin-using-well-known-key-timeout [trustCenterRejoinUsingWellKnownKeyTimeout:2]
- Sets the number of seconds to allow trust center rejoins for devices using the well-known key. A value of 0 means the policy should not be changed after a timeout. This must be called prior to forming or joining a network.
- trustCenterRejoinUsingWellKnownKeyTimeout - INT16U - The number of seconds that trust center rejoins will be responded to using the well-known link key.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_GET |
security mfg-token get
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_SET |
security mfg-token set [magicNumber:4] [value:2]
- magicNumber - INT32U
- value - INT16U