EmberAfClusterCommand Struct Reference
The EmberAFClusterCommand is a struct wrapper for all the data pertaining to a command which comes in over the air. This enables struct is used to encapsulate a command in a single place on the stack and pass a pointer to that location around during command processing.
#include <
af-types.h
>
Data Fields | |
EmberApsFrame * | apsFrame |
EmberIncomingMessageType | type |
EmberNodeId | source |
uint8_t * | buffer |
uint16_t | bufLen |
bool | clusterSpecific |
bool | mfgSpecific |
uint16_t | mfgCode |
uint8_t | seqNum |
uint8_t | commandId |
uint8_t | payloadStartIndex |
uint8_t | direction |
EmberAfInterpanHeader * | interPanHeader |
uint8_t | networkIndex |
The EmberAFClusterCommand is a struct wrapper for all the data pertaining to a command which comes in over the air. This enables struct is used to encapsulate a command in a single place on the stack and pass a pointer to that location around during command processing.
Field Documentation
EmberApsFrame* EmberAfClusterCommand::apsFrame |
APS frame for the incoming message
uint8_t* EmberAfClusterCommand::buffer |
uint16_t EmberAfClusterCommand::bufLen |
bool EmberAfClusterCommand::clusterSpecific |
uint8_t EmberAfClusterCommand::commandId |
uint8_t EmberAfClusterCommand::direction |
EmberAfInterpanHeader* EmberAfClusterCommand::interPanHeader |
uint16_t EmberAfClusterCommand::mfgCode |
bool EmberAfClusterCommand::mfgSpecific |
uint8_t EmberAfClusterCommand::networkIndex |
uint8_t EmberAfClusterCommand::payloadStartIndex |
uint8_t EmberAfClusterCommand::seqNum |
EmberNodeId EmberAfClusterCommand::source |
EmberIncomingMessageType EmberAfClusterCommand::type |
The documentation for this struct was generated from the following file:
af-types.h